This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22918: Datasheet equation typo?

Guru 19485 points
Part Number: TPS22918

About TPS22918 datasheet; page 19 and equation (9) ~ (13) are described CL: 22pF.

Is CL: 22pF typo and correct CL: 22μF?

Best regards,

Satoshi

  • Hello Satoshi-san, 

    Yes you are correct; based on the design requirements in the below table, the CL should be 22uF. 

    The resulting answer from the equations below will still be correct, but I will work to remedy this typo to avoid any confusion. 

    Thank you for bringing this to our attention. 

    Best Regards, 

    Elizabeth