Part Number: LM2941
Input pin of LM2941SX IN, ADJUST, ON / OFF
Could you tell me the absolute maximum rated voltage MIN value for each?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM2941
Input pin of LM2941SX IN, ADJUST, ON / OFF
Could you tell me the absolute maximum rated voltage MIN value for each?
Hi Yamaguchi-san,
We do not have that rating for the parts, but the operation of the part will be satisfied as long as the abs max is not exceeded. In this way, you may think of the abs max value as the MIN value.
IN - 60V
This is an older part and because of this we do not have any data on the abs max for these pins.
ADJUST - This pin should not be driven directly and as such should always be within 0-1.35V
ON/OFF - we do not have any defined limits for the voltage on the ON / OFF pin of this part.
Regards,
John
IN - 60V
Does the absolute maximum rating value of the IN pin match that it is ± 60V?
ON/OFF - we do not have any defined limits for the voltage on the ON / OFF pin of this part.
Does it mean that applying a voltage such as ± 15V does not affect the damage?
Hi Yamaguchi-san,
The input can go down to -75V
yes a ± 15V should be acceptable to apply to the ON/OFF pin of the part.
Regards,
John