Other Parts Discussed in Thread: UCD9222,
Hello,
I am working on a new design using the TMS320C6678ACYP DSP. For powering the CVDD and CVDD1 power rails I am using the UCD9222 and the UCD7242 following the TI application notes and the EVM schematic for the output capacitors on the UCD7242, both for capacitor values and the number of capacitors of each value. For these output capacitors, on the other side of the inductor from the UCD7242 SW-A and SW-B outputs, there is also a 1K ohm resistor. My question is: In what order should these components be physically placed on the PCB since some will be very close to the inductor and some will be somewhat further away? In the attached file “IC2002” is the UCD7242 and “IC2001” is the UCD9222. The figure in the attached document shows which components are closest to the SW-node inductor and which are further away. Is this the correct arrangement, or how should the physical placement be done?
Regards,
Larry