Hello Team,
is it possible to sync several TPS62913 on board with 2.2MHz from a CPLD? The duty cycle requirement in the datasheet is 45%-55% and CPLD output is 43%-57%. Is this going to be a problem or TPS has internal duty-cycle correction circuit?
Thanks and Best Regards,
Hans