Other Parts Discussed in Thread: TPS51200, TPS51200EVM
Hi team,
May I ask how customer could test TPS51200-Q1 sink current?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
May I ask how customer could test TPS51200-Q1 sink current?
Amelie,
To test sinking current, what you can do is something similar to the TPS51200EVM, where you connect a higher voltage source to the VTT output with low-value high-power resistors. On the EVM we use parallel 1.5ohm 1W resistors to accomplish this.
So, if you wanted to sink 1A of current with a 0.75 VTT and a 1.5V VLDOIN, you can connect VLDOIN to VTT with two parallel 1.5ohm 1W resistors.
It is important that these resistors have a high power rating due to the large V=IR drop across the resistors, which is why we recommend using parallel resistors.
Thanks,
Kadeem