Hello,
I having trouble getting same value for output inductor value by using formula from LMR16006 datasheet. Please refer to 9.2.1 Custom Design procedure.
Parameters:
Input Voltage: 16V
Output Voltage: 5.0V
Output Current 0.6 A
Switching Frequency: 0.7 MHz
On page 12 (9.2.2.2) for calculating output inductor selection, below formula is used to calculate:

Explanation for calculation Kind is confusing "... 30%-40% of the DC output current."
For example I chose 33% (with this percentage I got matching value)
- Should deduct Iout by 33% then Kind= 0.402 A and Lo= 0.00002036H
or
- Should get 33% of Iout then Kind= 0.198 A and Lo= 0.00004134
For me case 1 resulting value explained in datasheet, but does not follow common understanding of phrase "30%-40% of the DC output current."
What was value for Kind used in using formula 1 datasheet from page 12, where value of 20.4 µH is get as result?
Thanks,
Mladen