Other Parts Discussed in Thread: TPS2663, TPS2640EVM, TIDA-03031
Dear Sir, Madam,
in our application we want to develop a surge protection with TPS26600 and performance criterium A.
In App note SLVA833D the performance criterion B is described, criterion A has to be asked an application engineer.
Some more data about the supply voltage:
16.8V < VCC < 30.0V continous
14.4V < VCC < 33.6V for 100ms (no damage)
Transient test:
+-2KV
5/50ns puls
5KHz repetition freuquency
criterion A
Surge test:
+-2KV (Ri=42Ohm and 0.5µF) plus-line to earth and minus-liine to earth
+-1KV (Ri=42Ohm and 0.5µF) line to line
criteroin B
Could you please give an advise for performance criterion A?
Best regards
Thomas