Other Parts Discussed in Thread: TINA-TI
Hi,
1. For your datasheet here - https://www.ti.com/lit/ds/symlink/bq24308.pdf - is there a typo on page 14? I believe the PMOS is flipped, since the current as shown is going through the Drain to source direction.
2. Also, is your product compatible for the cases where a power supply may not be always connected (like in a battery scenario)?
3. Furthermore, can this product serve as a lithium cell protection circuit? Or should a separate protection IC be used? Any suggestions for such ICs are welcome.
4. For your example with the external PFET for reverse polarity protection, what would the voltage drop at the output be if the input power source is 5V? Seems your application example diagrams plot VIN (the input to the IC) not the input power source - so I wanted to better understand this.
5. Is there a spice model of this part for TINA-TI?
Thanks.