The BQ4050 RSOC jump at rom temperature.
1.The max error change 100% to 2% when charge and discharge current at 2000mA in the first cycle.
2.The RSOC is not jump when charge and discharge current at 1000mA in second cycle.
3.The RSOC is jump from 9% to 5% when charge and discharge current at 2500mA in third cycle.