Hi expert,
I have a question about TPS3808.
Is it possible to change the detected voltage using the Fixed Voltage Version of the TPS3808?
The Fixed Voltage Version in the Functional Block Diagram contains a 4MΩ resistor between the SENSE and GND pins.
Is it possible to change the detection voltage by placing a resistor between the power supply and the SENSE pin?
For example, in the case of TPS3808G33, it can be calculated that R1 is about 3.47MΩ and R2 is about 0.53MΩ, which are connected to the SENSE pin and GND pin.
If I want to detect 4V, should I put a resistor of about 1.23MΩ between the power supply and the SENSE pin?
Best regards,