This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A88: SCH review

Part Number: TPS7A88

Hi Team,

we are using TPS7A8801RTJT in our design and here is the schematic of it:

Out 1 is used to generate 0.85V from 1.8V input and Out 2 is used to generate 1.8V from 3.3V input.

Regarding Out 1, the feedback resistors selected are :

R1 as 750E and R2 as 12K. Is R1 value of 750E is fine ?

Also R3 and R4 is selected as 1.87K and 1.5K for 1.8V output as recommended in datasheet, table 2. 

--

Thanks in Advance,

Kiran