Dear Sir/Madam
Our customer wants to design a power supply using LM34966-Q1 with the following specifications.
Input voltage from a Li battery= 14.4V
Output voltage = 60V
However this seems to be impossible to simulate with the Webench, as the maximum output voltage allowed by the tool is 40V.
Nevertheless when looking at the datasheet this output value appears to be possible. Is this the case? If yes, is there any way to simulate it with Webench or any other calculation tool?
Thanks in advance and kind regards
Maria