This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62261-Q1: 1.8V at EM when power is off

Part Number: TPS62261-Q1

Hello,

Do you think it is OK if 1.8V is applied to VOUT (FB and SW pins) when the device power is off? The customer is considering applying 1.8V to the downstream circuit to activate it while the entire system power is off. I think it is OK for SW, but for FB the maximum rating is not defined.

Thank you.

Regards,

Oguri (TIJ automotive FAE)