This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS745: Is the device ok with surge from photodiode

Part Number: TPS745
Other Parts Discussed in Thread: LP3988, , TPS7A25, TPS7A20, TPS7A90

Hi Team

I have a customer asking me if we have any solution that supports the photodiode application with the following electrical requirements.

3.3V-2.8V, 115mA(LDO) with PG pin

I have found that the LP3988, TPS7A25 and TPS745 meets such requirements while having excellent cost/performance.

The problem is, however, as the customer is planning on using the LDO on the photodiode sensor, he mentioned that there would possibly be a surge generates by the photodiode as the CMOS sensor turns off, and he would prefer an LDO solution that's able to withstand such situation without needing to be turned off.

I don't have any information regarding how large the surge is but does TPS745(or LP3988, TPS7A25) look good for this kind of application? If not, some device suggestions would be much appreciated.

Regards

David