This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62125: TPS62125DSG

Part Number: TPS62125
Other Parts Discussed in Thread: TPS62170, TPS62160

Hi,

I use a TPS62125 in a design in inverting configuration for low consumption usage (4 mA max).

The inverted voltage have to be able to reach -9.4V with a Vin at 3.3V.

Our design well work till now but there is a shortage on the TPS62125DSG.

So I saw that TPS621260 and TPS621270 could be used as equivalency for TPS62125.
Could you confort me in this affirmation?

As on our design 4th pin Hysteresis is left unconnected, could AGND of TPS621260 and TPS621270 also be left unconnected or do we have to tie a strap?

Best regards,

Romain BORLET