Other Parts Discussed in Thread: TPS566231
Hello TI,
We are designing Boost and buck dc to dc converter.
we have few question,
1. If i configure(Design) boost convertor for input-8.4V/5A to output 12V/2.5A, In some condition if the input voltage goes beyond the 12V suppose its should be 15V then what is my output voltage TPS61288 or is it damage ..?
2. Same for buck converter if i configure (Design) Buck converter for input 5.4V/5A to output 5V/4A, If the voltage goes below the 5V, there is possibility drop down to 4.5V what is my output voltage TPS566231 or is it damage..?
Thanks,
Rahul