This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] LM388x: Is it good practice to connect EN pin to VCC?

Expert 4165 points


Connecting the EN pin to VCC is not recommended. During power up, the EN voltage should be kept below the EN threshold until VCC rises above the minimum operating voltage. An undefined operation at the FLAG outputs can occur if EN is connected to VCC.

For more LM388x FAQ click or type the tag in the search bar [FAQ] LM388x