Hi Team,
We have received this inquiry from our customer.
I need support on the REG103UA-3.3. I need details on how the foldback current works. I have an application that I had to add the 5K boost resistor and need to understand why. I have the LDO driving a GPS chipset (UBlox) and an external active GPS antenna. Depending on the cable length to the external antenna and number of adapters used, we get into a situation where the LDO does not start up. When I add the 5K ohm boost resistor from input to output, it functions normally. I need to be able to explain why this fix works and why it did not work in the original configuration. So, I need to know how the foldback protection works. If there are any application notes please include them.
Regards,
Danilo