How does PGTH function in TPS2663 ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Usually, PGTH is used to monitor the output voltage level so that PGOOD signal can be asserted to control the downstream load.
In TPS2663, PGTH is also used for fast transient recovery when voltage at PGTH is above PGTH threshold.
When PGOOD signal is not required, PGTH needs to connected to GND.