Hi, TI expert.
Customer is currently using ON-SEMI's FDD306P, and I'm going to review TI's CSD22205L.
The specs actually used in the board by the customer are as follows.
- Use Spec: Voltage - 4.3V / Current - 4A
Q1) It is judged that it can be used according to the spec on the datasheet, but since the package of CSD22205L is small, I would like the customer to check again whether there is any problem even if it is applied to the spec for use.
Q2) The maximum rating on the datasheet is -7.4A, but how many A can it actually be used?
Q3) Are there any precautions such as widening the pattern when applied to PCB?
Please Check. Thank you.