This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2662: Current after output cutoff

Part Number: TPS2662

CH1(Yellow) : Input+5V

CH2(Green) : Output+5V

CH3(Blue) : FLT

CH4(Red) : Output Current

Use TPS26620 Design Calculator

 VIN=5V、ILIM=0.3A、t(dVdV)=1.1ms

When a current of 2A is loaded, the output is cut off due to overcurrent, but even though the output voltage is 0V, the current remains about 0.3A.

Eventually, the current is also cut off. Is this possible?

I'm also using another eFUSE: TPS26601, but that doesn't happen.