CH1(Yellow) : Input+5V
CH2(Green) : Output+5V
CH3(Blue) : FLT
CH4(Red) : Output Current
Use TPS26620 Design Calculator
VIN=5V、ILIM=0.3A、t(dVdV)=1.1ms
When a current of 2A is loaded, the output is cut off due to overcurrent, but even though the output voltage is 0V, the current remains about 0.3A.
Eventually, the current is also cut off. Is this possible?
I'm also using another eFUSE: TPS26601, but that doesn't happen.