This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC3843A: IC heated after power up with 24 V DC or more than 15VDC

Part Number: UC3843A
Other Parts Discussed in Thread: UC3843

Hello

I'm using UC3843AD8 SOIC8 package IC for PWM generation. When I give power to IC it is getting worm on 12V . But when I was giving 24 Vdc power supply it is more heated .

Here is my schematic   IC are  more heated when give input to generate PWM 

Please suggest the changes in this schematic to avoid heating