Hi Team,
Usage conditions: TPS7A4701, Vin=24V, Vout=22V
Max value spec of Feedback pin current(Ifb) is not defined in the data sheet.
What is the estimated max value spec at operating temp range(-40℃ to +125℃)?
Best Regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Usage conditions: TPS7A4701, Vin=24V, Vout=22V
Max value spec of Feedback pin current(Ifb) is not defined in the data sheet.
What is the estimated max value spec at operating temp range(-40℃ to +125℃)?
Best Regards,
Hi Atsushi-san,
We do not have data for the max value of I_FB. It is recommended that you size the feedback resistors such that the ideal current flowing through them is at least 100 x I_FB. This will add enough margin that output accuracy is not effected by the non-ideal I_FB.
Regards,
Nick