This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65270: Difference VIN1 and VIN2 condition

Guru 19605 points
Part Number: TPS65270

Is different VIN1 and VIN2 condition have any problem?

Example pattern is below;

・Difference voltage, VIN1: 5V and VIN2: 12V

・Either one, VIN1: 12V and VIN2: 0V

・VIN startup timing differ, voltage supply sequence of VIN1→VIN2

Or, are there condition no problem because independent each power supply circuit?

Best regards,

Satoshi