This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM73605-Q1: What is the power consumption in standby mode of LM73605-Q1

Part Number: LM73605-Q1


Hi team,

What is the power consumption in standby mode of LM73605-Q1?

The data sheet is not clear, thank you

  • Hi Hazel,

    The standby IQ for VIN is 0.6 µA typical (with external bias)

    The standby IQ for the external bias is  21 µA typical.

    If there is no external bias then this will all be VIN current.

    The power will depend on VIN voltage and ext bias voltage.

    This is in section 7.5 of the datasheet.

    Hope this helps,

    -Orlando