Other Parts Discussed in Thread: CSD16406Q3
Hello,
I would like to run my protective circuitry design by you. I am using a 3P Grepow 704230 (835mAh) configuration that can charge at a maximum of 2505mA (1C) and discharge at a max rate of 7515(3C). The system needs to shut off under 2.8V and over 4.28V maximum. The two chips that came to mind are the BQ29707 and the BQ29737 because they are both either currently available or in the will be in the near future. Initially, I copied the basic design that was in the data sheet of the BQ297XX that uses the CSD16406Q3 mosfets. However, when the battery approaches 3V the on state resistance for the mosfet gets really high. Therefore, I was looking at the CSD16327Q3T as a replacement. Can you please take a look at my design and table that I used to this conclusion and let me know if my thinking is correct or not? (Ron is for two mosfets in series as in the design) Thank you.