Other Parts Discussed in Thread: BQ79616, ISO7742, ISO7742-Q1
Team,
The custom PCB has the below connection:
[BQ79616] (UART TX - pin 53) ---> (IN - pin 12) [ISO7742F DWR]
There is voltage on the BQ79616 UART TX line when in SHUTDOWN mode. This voltage seems to supplies the Isolator (ISO7742-Q1) with parasitic energy even though the VDD is disconnected from the Isolator supply.
And this makes the battery drains.
-Is the analysis correct?
-Is it a known issue?
-Can this be fixed someways?
Thanks in advance,
A.