Hello guys,
One of my customers is designing a power supply circuit using LM5155.
At this moment, they have the following questions.
Could you please give me your reply for them?
Q1. What is the minimum value of Cvcc as actual capacitance value? The device datasheet says that the recommended VCC capacitor value is from 1 μF to 4.7 μF.
Also TDK 1uF ceramic capacitor, GCM188R71C105MA64D is listed up as recommended parts.
The capacitor has +/-20% variation in production and +/-15% variation in temperature range.
So the minimum capacitance of the Cvcc is about 0.75uF. Can 0.75uF (Actual value) be used for Cvcc?
What is the minimum actual value of Cvcc?
Q2. Can a very small ESR ceramic capacitor be used for Cvcc. Is it no problem to use 1mohm ESR capacitor for Cvcc?
Your reply would be much appreciated.
Best regards.
Kazuya.