Other Parts Discussed in Thread: LM317
Dear sirs,
I am using the LM317A to have 37V at the output side with 48V at the input side. This should be possible according the specific regarding the input output maximum difference voltage in maximum ratings of data sheet. But in product details in Texas Instruments web site and in device comparison of data sheet the input voltage range is 4.25-40V so it seems i can't enter a voltage >48V.
Which of the two is correct?
Kindest regards
Stefano Casilli