Other Parts Discussed in Thread: TPS53353
Hello,
Is there a comparison table for the specifications of TPS53353/TPS53355?
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I do not believe we have a table similar to the one shared in the comments.
The TPS53353 and TPS53355 are pin to pin compatible devices that utilize the same controller. The TPS53353 is optimized for 20A or less and the TPS53355 is optimized for 20-30A applications. These parts are also Bom-to-Bom compatible with the possible exception of the current limiting resistor and the inductor (depending on application requirements).
Please reach out regarding any questions using the TPS53353 vs the TPS53355 in a particular application space.
Regards,
Alec Biesterfeld