Good morning,
I am trying to understand the soft start timing formula in the datasheet on page-14.
If I understand it correctly, It says 2.2uA charges the SS from 0.15V to about 0.8V for the handoff of the SS voltage to reference voltage.
given Formulla-> Css( nF) = 3 x Tss(mS).
For example If I have a 3N3 %10 capacitor connected to SS pin, then I expect to see 1.1ms with a %10 tolerance as a soft start time. How shall I correlate this to output voltage rise time?
I assume this formula is a rough formula and I need to take into account the tolerances of reference voltage and tolerances of Iss which charges the external slow start capacitor to calculate the soft start time?
Thanks in advance for your help,
Best regards
Onur