Other Parts Discussed in Thread: TPS7A11
Hi,
TLV755P is used in my customer's new projects. But it is found that the max value of “EN pin low voltage” is too small, so that there is a risk. Could you please help?
1, Are there alternatives with a larger upper limit and small size (less than 1.5mm2)? I noticed that TPS7A11 may be an option, but the value is only 0.4V.
2, Why are the max value of “EN pin low voltage” of many LDOs so small? Are there any benefits?
3, Besides, TPS7A11 has BIAS pins. What is the benefit or function? When there is no additional bias power supply, should BAIS be connected to IN?
Many thanks!