Hi Team,
My customer wants to control the charging current as follows.
Is it possible for BQ25155 to control?
Ta=0~15℃: 9mA
Ta=15~45℃: 135mA
Best Regards,
Yaita
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Yaita,
Yes, with the BQ25155 the customer could configure, then read the ADC_DATA_TS (0x44) registers to obtain the TS temperature reading, and then take any action on their software to change the fast charge current ICHG_CTRL (0x13) to 8.75mA on 0-15C and to 135mA on 15-45C range. Additionality, they can also configure the ADC comparators to trigger interrupts at the temperature thresholds crossing to notify the MCU to take any required action.
Best regards,
Arelis G. Guerrero