Hi, support team
My customer has the questions as follow:
In my design: input VIN = 2.5V, output VOUT = 1.8V, ICL = 80%
1. Which value should I choose for VFB_PG(typ) in Equation 3 when I calculate RFB_PG(TOP) and RFB_PG(BOTTOM) according to Equation 3?
0.2V? or 0.21V? or (VIN-VDO)~0.2V in Note1?
2. How is the PG threshold parameter calculated in table 9-1?
Thanks so much.
Best regards,
Yuki