This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25180-Q1: operation mode and frequency

Part Number: LM25180-Q1
Other Parts Discussed in Thread: LM5180

Hi Expert,

Our customer uses LM25180-q1 for insolated 12V@12V in HV BMS. The max output current is 0.1A. Now they want to which operation mode and frequency it work at. I have a few questions about this.

1. how much is the rated output power? 7W?

2. do you have an exact number of % of the division between FFM and DCM?

3.How is the EMC performance of these three mode? Which one is the best? 

Thanks A lot!

Elec Cheng