This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25601D: Charging low capacity batteries

Part Number: BQ25601D
Other Parts Discussed in Thread: BQ25618, BQ25611D

This device is used to charge batteries in the range 150 mAh to 2400 mAh. There is now a requirement to charge 45 mAh batteries but the lowest charge current and pre conditioning charge current are too high for this battery. Is there a way that the BQ25610D can be configured reducing the charge current below 60 mA?