This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40055: Question about change the current limit point.

Part Number: TPS40055

Hi

I wanna change the current limit point.

I did it like a calculation formula, but it can't be changed.

Therefore, there is no change even if the ILIM resistance is changed to 1Kohm~10Mohm.

Do I have to change other parts besides resistance?

Thanks

  • Hi David 

    If the current limit level is lower than your expectation and it doesn't change by changing RILIM, It might be caused by a noise injection. 

    If the current limit level is higher than your expectation and it doesn't change by changing RILIM, it might be cause by a wrong connection on your layout 

    Please refer the equation (16) in the datasheet.  

    - Eric Lee ( Applications Engineering) 

  • Hello
    I am closing this thread since I have not heard from you for sometime.
    If you are still trying to resolve the issue, please feel free to open a new thread or reopen this thread. Thanks
    - Eric Lee (Applications Engineering)