Other Parts Discussed in Thread: LMR16010, LM76002
Hi sir,
I am using ADJ version for 24V input and - 15V output.
The input capacitor of 330 uF electrolytic capacitor and 2.2 uF SMD cap are connected in parallel.
Output inductor 220 uH.
The 1.23V input to the FB terminal and use 27Kohm and 2.4Kohm as voltage divider resistance .
The output capacitor have 3pcs 10uF in parallel connection.
What is the selection of the feedforward capacitor for phase compensation at this time?
(capacity, rated voltage, temperature characteristics, frequency characteristics, etc.)
In particular, I want to know what the capacity is and what the rated voltage is above.
Thank you for your suggestion.
Regards,