Hi Team,
I believe toggling #MR pin doesn't reset the registers of BQ25155.
Is my understanding correct?
Could you tell me the cases that resets registers to default value?
Best Regards,
Yaita
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
I believe toggling #MR pin doesn't reset the registers of BQ25155.
Is my understanding correct?
Could you tell me the cases that resets registers to default value?
Best Regards,
Yaita
Hi Yaita,
The cases that'll reset the registers are:
The MR can be configure to do a hw reset or to enter/exit shipmode. So toggling the MR under the right conditions can cause the registers to go back to default.
Best regards,
Arelis G. Guerrero
Hi Arelis-san,
Thank you for your clear explanation.
>4. Doing a full power cycle (remove battery and VIN)
Could you tell me the threshold battery voltage that can cause the registers to go back to default?
I assume VIN isn't applied in this case.
Best Regards,
Yaita
Hi Yaita-san,
Assuming no VIN, the threshold for battery will be when VBAT < VBATUVLO. Default BATUVLO is 3.0V, but you can change it on the BUVLO Register (0x16).
Best regards,
Arelis G. Guerrero