Hell expert,
This is Koki Tsushima and received questions from customer.
Could you answer for questions?
, from page 10
Q.1 Could you tell me the min and typ of HW reset watchdog timer?
Q.2.1 How many second was the PMID powered off after 14-seconds watchdog timer when without interference by I2C?
Q.2.2 When the Q.2.1 case, how will be the register?
I think watch dog timer will be reset, but is this meaning that the register goes into default?
Q.3.1 Is this HW reset watchdog timer be activated just when there is Vin?
Will not this HW watchdog function if HWRESET_14S_WD=1(enable) or HWRESET_15S_WD=1(enable) without Vin?
Q.3.2 What is the meaning of WATCHDOG_15S_ENABLE on first table?
There are no mentions except on this table.
Was it 0x37H[2:1] HWRESET_14S_WD?
This register should be related on Q.3.1.
Q.4 Will it SW watchdog function without Vin?
Q.5 Is this understanding for HW reset watchdog timer function correct?
- If there are I2C within 14-seconds, the timer should be updated.
- If there are next I2C within 14-seconds again, the timer should be updated.
Was it updated eternity for that case?
Q.6 Is this understanding for HW reset watchdog timer function correct?
When there are no I2C within 14-seconds, PMID was turned off and watchdog error.
For that case, will this error be solved by HW reset or USB Insertion / removal?