Hi,
In an LM3477 Inverting Buck Boost configuration where the IC ground is negative voltage referenced and sinking current, what is the correct current sense configuration? In the buck configuration, the sense resistor is between VIN and the source of the nmos, and the designed voltage drop across the sense resistor is inputted into the "current limiting internal circuitry" as seen below.

Looks like the internal "short circuit detect" and "PWM" comparators are both referenced to a proportional gain-VIN hence a nominally higher voltage than the ISEN pin after the sense resistor voltage drop. There are some IC-ground-referenced current sources which would be negative-voltage referenced in an IBB. Hence, as current would still be sunk into the lower voltage node, system ground, and the fact that the IC is sinking current is independent of the positioning of the current sense resistor in this configuration as the current control circuitry operates assuming still a current drain from its perspective? In summary, nothing changes in terms of the current sense resistor topology in the LM3477 IBB.