This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92663A-Q1: UART COMMUNCTION

Part Number: TPS92663A-Q1


refer to the follow pciture:could i use it like this ?

there any two pcb and two IC ,could i only use one CAN TR? the two IC not on the same one PCB,so Does this result in data loss?

  • Lei,

    Thanks for your question. This device is gated and the datasheet is not public. Therefore any discussions related to product details should be done over email and not over this public forum.

    Please reach out to us via email. Have you already requested access to the full datasheet via mySecure?

    Thanks

    Caroline