Other Parts Discussed in Thread: TLV1117, TLV767
Hi team,
My customer want to get the recommend LDO socket to replace NCP1117ST12T3G.
could you please help to check this case?
Thank you very much!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Chen,
Unfortunately, we don’t have a fixed 12V option that is p2p. TLV1117 and TLV767 adjustable options would be the best replacement devices here. TLV767 is our newest device with better performance. Please let us know if you have any questions.
|
|
NCP1117 |
TLV1117 |
TLV767 |
|
AEC Q100 |
NO |
NO |
NO |
|
Output Options |
Adjustable Output, Fixed Output |
Adjustable Output, Fixed Output |
Adjustable Output, Fixed Output |
|
Iout (Max) (A) |
1 |
0.8 |
1 |
|
Vin (Max) (V) |
20 |
15 |
16 |
|
Vin (Min) (V) |
2.7 |
2.7 |
2.5 |
|
Vout (Max) (V) |
18 |
13.7 |
14.5 |
|
Vout (Min) (V) |
1.25 |
1.25 |
0.8 |
|
Fixed Output Options (V) |
1.5, 1.8, 1.9, 2, 2.5, 2.85, 3.3, 5, 12, ADJ |
1.5, 1.8, 2.5, 3.3, 5 |
0.8, 1.8, 2.8, 3.3, 5 |
|
Enable |
NO |
NO |
YES |
|
Power Good |
NO |
NO |
NO |
|
Output Capacitor Type |
Ceramic |
Non-Ceramic |
Ceramic |
|
PSRR @ 100KHz (dB) |
40 |
28 |
53 |
|
Noise (uVrms) |
540 |
411 |
60 |
|
Accuracy (%) |
2 |
3.75 |
1 |
|
Vdo (Typ) (mV) |
1200 |
1200 |
900 |
|
Iq (Typ) (mA) |
3.6 |
1.7 |
0.05 |
|
Thermal Resistance θJA (°C/W) |
67 |
28 |
60.1 |
|
Min Package Area (mm2) |
22.75 |
16 |
4 |
|
Package Type |
SOT-223, TO-252 |
DDPAK/TO-263, SON, SOT-223, TO-220, TO-220, TO-252 |
HVSSOP, WSON |
Thanks,
Prakash L