Other Parts Discussed in Thread: BQ25731
Hi,
We are considering replacing BQ25731 with BQ25730 by referring to the thread below.
https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1053359/bq25730-about-vsys-voltage-control-when-batfet-is-not-used/3897374#3897374
Customer is verifying by replacing BQ25731 with BQ25730.
As a result, the phenomenon that the current consumption of BQ25730 became larger than that of BQ25731 occurred.
For both BQ25730 and BQ25730, the default registers are rewritten as follows.
Under this setting condition, BQ25731 was on the order of several tens of μA.
On the other hand, BQ25730 was on the order of several hundred μA.
Is there a way to reduce the current consumption of BQ25730?
And Could you give me some advice on the cause of the increase in current consumption?
ChargeVoltage | 05/04h | 16.608V:40E0h |
ChargeCurrent | 03/02h | 0000h |
OTGVoltage | 07/06h | 0000h |
OTGCurrent | 09/08h | 0000h |
IIN_HOST | 0F/0Eh | 1B00h @10mΩ |
ChargeOption0 | 01/00h | E31Bh |
ChargeOption1 | 31/30h | 3300h |
ChargeOption2 | 33/32h | 00BAh |
ChargeOption3 | 35/34h | 0434h |
ChargeOption4 | 3D/3Ch | 0040h |
ProchotOption0 | 37/36h | 0A81h |
ProchotOption1 | 39/38h | 1900h |
ADC Option | 3B/3Ah | 2040h |
Best regards,
Yusuke