Hi,
Im currently experimenting with the LMG5200 for use in a class D audio amplifier.
There is no finished circuit yet, I've only done some preliminary testing by feeding a sine wave and a sawtooth into a comparator with complimentary outputs. That then goes into two buffers with an RC element for dead time.
This works fine for some time -maybe a minute- before the LMG5200 fails.
This happened FOUR times !
On three of these, VIN is permanently shorted to SW. On one, VIN, SW and PGND are shorted.
I have no idea what went wrong. I also fail to understand why it always works for some amount of time and then fails suddenly.
Searching online, this seems to be a common problem with the LMG5200, but I could figure out why.
Given the price of these parts, this is incredibly infuriating.
Any Ideas ?