Part Number: LM5041A
Other Parts Discussed in Thread: LM5041,
Use LM5041 as a current-fed push-pull topology, use an external error amplifier, disable the internal error amplifier, and ground the FB pin of LM5041; in the initial stage of power-up, the output voltage of the error amplifier and the REF pin voltage rise at the same time, causing the REF pin to output The voltage is only about 1.86V, but cannot reach 5V, causing the entire chip to fail to work normally. May I ask what causes this? How to deal with it?



This is the voltage waveform of the REF pin and the COMP pin when the power is turned on. Yellow waveform: REF pin voltage waveform. Blue waveform: COMP pin voltage waveform. Purple waveform: The output waveform at pin 1 of the error amplifier. It can be seen that after power-on, the COMP voltage has already been established, while the REF voltage has been established relatively late. After C42 is increased to 1uF, it can start normally, but C42 cannot be designed to such a large capacity, which affects the control loop. You help me analyze what is the problem? I feel that when the LM5041 is powered on, there are certain requirements, but they are not written in the datasheet. In addition, after this circuit is powered on, short-circuit the COMP pin to ground for a short time, the REF pin voltage can immediately rise to 5V, and the chip can work normally.

Yellow waveform: +11V main power supply waveform. The UVLO threshold voltage of LM5041 is designed to be 12.3V. Blue waveform: REF pin voltage waveform. Purple waveform: COMP pin voltage waveform. The +11V power supply is a BUCK-type DC DC step-down power supply. It can be seen from the figure that the startup process is slightly slower. The power supply part of the circuit in the figure below, the power supply of the error amplifier comes from +6VA.