This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Buck-Boost parts recommendation inquiry

Other Parts Discussed in Thread: TPS631000, TPS63802, TPS63100

Hi, TI expert.

There is a Buck-Boost inquiry from a customer.

Specifications are as follows.

-------------------------------------------------------------------------------------------------------------------------

- Application : Rechargeable RCU(Remote control unit) with LIC battery (Li-ion capacitor)

- Vin : 1.5V ~ 5V

- Vout : Typ. 3.3V

- Load current : Max 700mA

- Need to Enable/disable control pin

- Low quiescent current

- Package: Excluding LGA and BGA package types

-------------------------------------------------------------------------------------------------------------------------

Are there any suitable parts? Please recommend.

Please check. Thank you.