Hi,
I connected 12v battery to BQ34110EVM, with these settings, 16V is selected in J5 connector and >5v in J2 connector. I also gave 3.3V to VEN pin in J6 connector with LOAD, VEN and J4 headers in default state. What else should be connected in the board. These connections are understood from TRM only.
What is the role of R21 resistor in EVM?