This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3489-Q1: Request to check the circuit

Part Number: LM3489-Q1
Other Parts Discussed in Thread: PSPICE-FOR-TI

I would like you to check the circuit.

Input voltage: 5 V, 9 V, 15 V, 20 V

Output voltage: 5V, 9V, 15V, 20V

Output current: 3A (MAX) It is designed according to the circuit diagram of TPS65988EVM.

However, use a ceramic capacitor for the output capacitor. I checked "8.2.2.2 Output Capacitor Selection (COUT)", It says that you have to insert a series resistor, Where and how many Ω resistance values should I put in?